CT Training London

Level II Training in London for Cardiac Computed Tomography

This training is designed to provide case volume, formal education, and hands-on training.  

Bilateral severe emboli can be shown in para-coronal VRT.

Flash CT Pulmonary Angiography in a Freely Breathing Patient

The CT pulmonary angiography showed a partially occlusive massive bilateral pulmonary embolism and signs of right heart strain.  

Sagittal MPR demonstrates an ill-defined soft tissue mass in the supra sternal region, anterior to the sternum (Fig. 1A).

Dose Reduction Combining CARE Dose4D, CARE kV and SAFIRE Techniques

A thorax and abdomen contrast CT scan was performed, which demonstrated an ill-defined soft tissue mass in the supra-sternal region, anterior to the sternum with asymmetrical thickening of the major pectoral muscle.  

eNews_CT_PortugalMummy_Release.pdf - Adobe Acrobat Pro

Egyptian Mummy Diagnosed with Prostate Cancer

The oldest known case of prostate cancer in ancient Egypt has been diagnosed in Lisbon, Portugal using Siemens computed tomography (CT) scanning techniques.  

VRT of the left coronary artery shows the soft tissue mass surrounding the vessel (arrow).

SOMATOM Definition Flash: Ruling out Coronary Artery Disease and Diagnosing Coronary Arteritis with 1.3 mSv

Coronary CT Angiography is a wellestablished method to rule out coronary artery disease.  

Flash-Scanner

Faster Cardiovascular Reading with the CT Cardio-Vascular Engine

SOMATOM Definition Flash and syngo.via integrated into PACS provide fast and efficient image management in daily cardiologic routine.  

Barasaurus besairiei

Frankfurt Constructional Morphology revised and applied in a study on the procolophonoid Barasaurus besairiei

Investigation of a 255million year old crime scene- studies on Barasaurus.
In the course of his diploma thesis, a student of paleontology from the Geozentrum Nordbayern in Erlangen executed a study on two specimens of the 255mio year old Madagascan Reptile Barasaurus besairiei, which were provided as a loan from the stock of the Staatlichen Museum für Naturkunde Karlsruhe. With the help of Siemens, the circumstances of death and fossilization of the animals could be reconstructed.